JM Badge Board Bootloader Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JM Badge Board Bootloader Problem

ソリューションへジャンプ
2,275件の閲覧回数
SvmPrasad
Contributor I

Hi,

 

When I connect my JM Badge board to Computer's USB, it runs the message "Press E4 for Bootloader" continuously. After pressing E4 key, left 4 columns of LED light up.

 

After downloading the .S19 file it doesn't work properly.

 

Regards,

SVMP

 

 

 

Message Edited by svmp on 2009-12-09 04:33 AM
ラベル(1)
0 件の賞賛
返信
1 解決策
1,460件の閲覧回数
mnorman
NXP Employee
NXP Employee

It sounds like the main application is broken.  The bootloader message "Press E4..." will timeout and attempt to start the application if you do not press E4 soon enough.  It sounds like it is trying to start this application and failing, which resets the hardware and it starts over with bootloader.  Did you follow the steps as outlined in this post to reprogram the original image?

 

Message Edited by mnorman on 2009-12-16 08:41 PM
Message Edited by mnorman on 2009-12-16 08:43 PM

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,461件の閲覧回数
mnorman
NXP Employee
NXP Employee

It sounds like the main application is broken.  The bootloader message "Press E4..." will timeout and attempt to start the application if you do not press E4 soon enough.  It sounds like it is trying to start this application and failing, which resets the hardware and it starts over with bootloader.  Did you follow the steps as outlined in this post to reprogram the original image?

 

Message Edited by mnorman on 2009-12-16 08:41 PM
Message Edited by mnorman on 2009-12-16 08:43 PM
0 件の賞賛
返信