Is the InterNiche’s ColdFire TCP/IP Stack compatibe with the MCF5225X?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is the InterNiche’s ColdFire TCP/IP Stack compatibe with the MCF5225X?

ソリューションへジャンプ
1,536件の閲覧回数
m4l490n
Contributor V

Hi

I was wondering if the TCP/IP stack is compatible with the Coldfire V2 MCF5225X family because I have the MCF5225X Tower Board and I don't want to use the MQX because it's lack of functionality, particularly regarding peripheral drivers, and I want to use processor expert to develop my projects.

Thank you!!

0 件の賞賛
返信
1 解決策
1,336件の閲覧回数
butok
NXP Employee
NXP Employee

Hi Manuel,

Just in case, if you have an issue with InterNiche "MCF5225X family" support, you can look at FNET Embedded TCP/IP stack http://fnet.sourceforge.net

Best regards,

Andrey

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,337件の閲覧回数
butok
NXP Employee
NXP Employee

Hi Manuel,

Just in case, if you have an issue with InterNiche "MCF5225X family" support, you can look at FNET Embedded TCP/IP stack http://fnet.sourceforge.net

Best regards,

Andrey

0 件の賞賛
返信