Is the InterNiche’s ColdFire TCP/IP Stack compatibe with the MCF5225X?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is the InterNiche’s ColdFire TCP/IP Stack compatibe with the MCF5225X?

跳至解决方案
1,129 次查看
m4l490n
Contributor V

Hi

I was wondering if the TCP/IP stack is compatible with the Coldfire V2 MCF5225X family because I have the MCF5225X Tower Board and I don't want to use the MQX because it's lack of functionality, particularly regarding peripheral drivers, and I want to use processor expert to develop my projects.

Thank you!!

0 项奖励
回复
1 解答
929 次查看
butok
NXP Employee
NXP Employee

Hi Manuel,

Just in case, if you have an issue with InterNiche "MCF5225X family" support, you can look at FNET Embedded TCP/IP stack http://fnet.sourceforge.net

Best regards,

Andrey

在原帖中查看解决方案

0 项奖励
回复
1 回复
930 次查看
butok
NXP Employee
NXP Employee

Hi Manuel,

Just in case, if you have an issue with InterNiche "MCF5225X family" support, you can look at FNET Embedded TCP/IP stack http://fnet.sourceforge.net

Best regards,

Andrey

0 项奖励
回复