Is the InterNiche’s ColdFire TCP/IP Stack compatibe with the MCF5225X?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the InterNiche’s ColdFire TCP/IP Stack compatibe with the MCF5225X?

Jump to solution
1,541 Views
m4l490n
Contributor V

Hi

I was wondering if the TCP/IP stack is compatible with the Coldfire V2 MCF5225X family because I have the MCF5225X Tower Board and I don't want to use the MQX because it's lack of functionality, particularly regarding peripheral drivers, and I want to use processor expert to develop my projects.

Thank you!!

0 Kudos
Reply
1 Solution
1,341 Views
butok
NXP Employee
NXP Employee

Hi Manuel,

Just in case, if you have an issue with InterNiche "MCF5225X family" support, you can look at FNET Embedded TCP/IP stack http://fnet.sourceforge.net

Best regards,

Andrey

View solution in original post

0 Kudos
Reply
1 Reply
1,342 Views
butok
NXP Employee
NXP Employee

Hi Manuel,

Just in case, if you have an issue with InterNiche "MCF5225X family" support, you can look at FNET Embedded TCP/IP stack http://fnet.sourceforge.net

Best regards,

Andrey

0 Kudos
Reply