Interrupt 5275EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interrupt 5275EVB

3,943 Views
bizio
Contributor I
Hi all,
I'm working with 5275EVB.I have a problem with the management of the interrupts generated by the UARTs. The source code used to inizialize the UARTs is the following:

MCF_UART_UCR1 = MCF_UART_UCR_RESET_TX;
MCF_UART_UCR2 = MCF_UART_UCR_RESET_TX;

MCF_UART_UCR1 = MCF_UART_UCR_RESET_RX;
MCF_UART_UCR2 = MCF_UART_UCR_RESET_RX;

MCF_UART_UCR1 = MCF_UART_UCR_RESET_MR;
MCF_UART_UCR2 = MCF_UART_UCR_RESET_MR;

MCF_UART_UMR1 = (0
| MCF_UART_UMR_PM_NONE
| MCF_UART_UMR_RXIRQ
| MCF_UART_UMR_BC_8 );
MCF_UART_UMR2 = (0
| MCF_UART_UMR_PM_NONE
| MCF_UART_UMR_RXIRQ
| MCF_UART_UMR_BC_8);

MCF_UART_UMR1 = (0
| MCF_UART_UMR_CM_NORMAL
| MCF_UART_UMR_SB_STOP_BITS_1);
MCF_UART_UMR2 = (0
| MCF_UART_UMR_CM_NORMAL
| MCF_UART_UMR_SB_STOP_BITS_1);

MCF_UART_UCSR1 = (0
| MCF_UART_UCSR_RCS_SYS_CLK
| MCF_UART_UCSR_TCS_SYS_CLK);
MCF_UART_UCSR2 = (0
| MCF_UART_UCSR_RCS_SYS_CLK
| MCF_UART_UCSR_TCS_SYS_CLK);


MCF_UART_UIMR1 = MCF_UART_UIMR_RXRDY_FU;

MCF_UART_UISR1 = MCF_UART_UISR_RXRDY_FU;

MCF_UART_UIMR2 = MCF_UART_UISR_RXRDY_FU;

MCF_UART_UISR2 = MCF_UART_UISR_RXRDY_FU;


ubgs = (uint16)((SYSTEM_CLOCK*1000000)/(9600 * 32));

MCF_UART_UBG1(1) = (uint8)((ubgs & 0xFF00) >> 8);
MCF_UART_UBG2(1) = (uint8)(ubgs & 0x00FF);

ubgs = (uint16)((SYSTEM_CLOCK*1000000)/(4800 * 32));

MCF_UART_UBG1(2) = (uint8)((ubgs & 0xFF00) >> 8);
MCF_UART_UBG2(2) = (uint8)(ubgs & 0x00FF);


MCF_UART_UCR1 = (0
| MCF_UART_UCR_TX_ENABLED
| MCF_UART_UCR_RX_ENABLED);
MCF_UART_UCR2 = (0
| MCF_UART_UCR_TX_ENABLED
| MCF_UART_UCR_RX_ENABLED);

At the beginning it runs correctly, but after some interrupts received the CodeWarrior goes on error.
The error is "Address Error".
Someone can help me to resolve this error?
Thank you in advance for your help.

Message Edited by bizio on 2006-06-19 03:17 AM

Labels (1)
0 Kudos
Reply
2 Replies

1,591 Views
mvincent
Contributor I
Something to check: make sure you have programmed the interrupt controller's ICRs with unique interrupt level/priority. Also, make sure all the code and structures involved in the service routines are reentrant or in critical sections.
0 Kudos
Reply

1,591 Views
fire
Contributor I

hai,

I faced the same problem and i strugled for days.

The problem is with nesting of interrupts.If u are disabling the global interrupt any where, do it in the correct way.

let me know whether you are disabling the interrupts any where.Give me the correct details.

ALL THE BEST.

0 Kudos
Reply