Intermittent USB Recognition Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Intermittent USB Recognition Issue

跳至解决方案
2,080 次查看
grt951
Contributor II

I am using the freescale USB CDC stack and virtual com port driver for the MCF51JE256 as a device only and have a intermittent issue where windows will not recognize the device. The hardware is to the USB app note (33ohm series resistors and 1.5k pull-up on D+) and the device will recognize roughly 50% of the time. It seems to also be PC dependent which is why I am looking at the hardware...any ideas?

 

Thanks,

 

Gary

EE

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,940 次查看
grt951
Contributor II

Hi Pepe,

Thanks for the info...we have resolved the issue the internal VREG was not being supplied with the correct voltage via VBUS causing a inconsistent signal.

Thanks...

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,940 次查看
Pepe_Ruiz
Contributor IV

Hi Gary,

Are you using an external 1.5K ohm resistor or the internal one?

If you use an external one you are not giving enough time to the MCU to enable properly the internal PLL and all the USB stack. remove the external pull-up resistor. the MCU already has an internal resistor that will be activated in SW.

try it and let us know if worked.

regards

1,941 次查看
grt951
Contributor II

Hi Pepe,

Thanks for the info...we have resolved the issue the internal VREG was not being supplied with the correct voltage via VBUS causing a inconsistent signal.

Thanks...

0 项奖励
回复