Improved FTP support for uTasker M5223X project - new doc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Improved FTP support for uTasker M5223X project - new doc

3,496 Views
mjbcswitzerland
Specialist V
Hi All

For uTasker users and anyone else interested - improved FTP support has been added to the uTasker M5223X project which will be available in the next SP.
This ensures compatibility with various 'favourite' FTP clients including FireFTP (FireFox with add-on) in active and passive modes with anonymous or authentication login.

The following new document details the implementation (requiring 4,5k program space on the M5223X) with an overview of FTP operation as well as practical FTP client comparisons.

http://www.utasker.com/docs/uTasker/uTaskerFTP.PDF

Questions and comments are welcome.

Regards

Mark Butcher

www.uTasker.com

Labels (1)
0 Kudos
Reply
3 Replies

1,725 Views
mjbcswitzerland
Specialist V
Hi All

Here is a quick update.

The Service Pack SP4 is now available to all uTasker users on the V1.3 SW page
http://www.utasker.com/software/softwareV1.3.html
A complete list of service pack additions is given at
http://www.utasker.com/software/V1.3/SP_M5223X_Notes.txt

At long last this SP is supplied with a GNU build project (as well as CodeWarrior) which works great!! It can be build from VisualStudio when working with the uTasker simulator. Here is a direct comparison of code sizes...showing just how competive the GNU compiler is!
GNU   FLASH    56'848 bytes / RAM 1'728 bytes (including 1024 bytes for vector RAM)
CW6.3 FLASH    59'492 bytes / RAM 1'680 bytes (including 1024 bytes for Vector RAM)
For anyone with a M52233DEMO or M52235EVB I have updated an SREC of the standard project demo which shows FTP, HTTP and Telnet capabilities which can be found here:
http://www.utasker.com/software/software.html

Don't forget that the uTasker is completely free for non-commercial use and new users are always welcome.

Regards

Mark Butcher

www.uTasker.com
0 Kudos
Reply

1,725 Views
mjbcswitzerland
Specialist V
Hi All

Please note that up to date documentation and information about the uTasker project can be found on the uTasker web site www.uTasker.com.

From the beginning of July 2007 the uTasker has its own forum for discussions and questions!!

Regards

Mark
0 Kudos
Reply

1,725 Views
mjbcswitzerland
Specialist V
Hi All

Please note that the uTasker forum switched live on 9.7.2007.
There is a Coldfire M5223X forum category and you are all most welcome to check it out or become an active forum member.

Regards

Mark

www.uTasker.com
0 Kudos
Reply