Illegal stack type!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Illegal stack type!

2,177件の閲覧回数
b_iglesias
Contributor I
After copying my code from ROM to RAM and execute it, everything seems to work except that I have got lots of "Illegal stack type!" and "User Defined Vector 0" exceptions. I didn't find any information about what could cause this.

Can someone help me ?
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,443件の閲覧回数
ericp
Contributor I
Hi,
 
I have the same problem with a MCF5485, but I can't find the answers to the previous post.
Somebody knows the reason please ?
 
Thanks
 
0 件の賞賛
返信

1,443件の閲覧回数
Alban
Senior Contributor II
Hi Eric,

When trying to get help from the Community it is better to give as much details as possible.
I am not a ColdFire expert however, for someone to answer, we usually need:
- Device,
- CodeWarrior version if CodeWarrior is linked to the problem,
- a piece of code if pertinent,
- schematics if pertinent...

In fact, the more information are available, the more chances you have to get a reply.

Otherwise, you still have the possibility to create an formal request for help by creating a service request (see link in my signature).
The main difference is that there is no guarantee of answer on the Forum.

Cheers,
Alban.
0 件の賞賛
返信