I2C to extend RAM from 52259?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C to extend RAM from 52259?

1,731 Views
JaimeR
Contributor III

I am just wondering if it's possible to extend the internal RAM by connecting an external RAM into I2C

using 52259 MCU.

If it's possible, what kind of RAM memory should I use?

If not possible, what are my options in order to extend RAM?

 

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

926 Views
admin
Specialist II

The answer strongly depends on the kind of external RAM access speed you need to have. A write or read access to on-chip RAM takes 1 CPU cycle. It will take around 100 us to transfer 32 bits of data across I2C (at 400 kHz I2C speed) - that is 8000 CPU cycles at 80 MHz CPU clock. It's up to you to decide if it is acceptable for your application.

The datasheet says that on 144-pin packages, the Mini-FlexBus interface is available. It should support glueless connection to static RAM chips. Access speeds would on the order of tens of CPU cycles. The advantage of this approach is that you would be able to map variables in your program directly into external memory.

You could also use GPIO pins to emulate an external memory interface. That would be slow too.

0 Kudos
Reply