I2C Problem with MCF525, only first I2C bus works, second NOT.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C Problem with MCF525, only first I2C bus works, second NOT.

1,344 Views
MdeJong
Contributor I
Hello,
 
I have a problem with the second I2C bus on the MCF5251,
the first I2C bus is working correctly, but the second I2C bus isn't working at all.
 
The initializing routines for the I2C busses are the same.
This I2C bus is working fine.
 
All the routines are the same, only the register base is different.
 
Am I doing something?
 
Regards Mark,
 
Labels (1)
0 Kudos
Reply
1 Reply

716 Views
JimDon
Senior Contributor III
Did you correctly set the pin function register for the second I2C module?

0 Kudos
Reply