How to use CW_MCU_v11.1_b181224_PE software compiler through the command to compile a project i

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use CW_MCU_v11.1_b181224_PE software compiler through the command to compile a project i

1,848 Views
wwj
Contributor I

In Win10, I want to call CW_mcu_v11.1_b181224_PE software compiler by a command to compile a project. Do I need to compile a batch file? How do I write this file?

0 Kudos
Reply
1 Reply

1,840 Views
TomE
Specialist II

I think you would be better off asking this question in one of the two CodeWarrior forums. These are a bit hard to fins as they don't show up in the main list of forums??? They can be found on that page by searching for "codewarrior".

There should be an option somewhere on this page (under one of the menus?) to MOVE your post to another forum. Or maybe a Mod has to do it now. Anyway:

https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/bd-p/cw-classic

https://community.nxp.com/t5/CodeWarrior-for-MCU/bd-p/cw-mcu

Tom

 

0 Kudos
Reply