How to know what´s the bus frequency of my MCU - Using DEMOQE128 board and MCF51qe

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to know what´s the bus frequency of my MCU - Using DEMOQE128 board and MCF51qe

跳至解决方案
3,325 次查看
jreyes085
Contributor I

Hi,

 

I want to know How to know what´s the bus frequency of my MCU - Using DEMOQE128 board and MCF51qe...

 

I already programmed this, and made test with the oscilloscope to see the frequency output of a blinking led that the board has...i obviously counted the number of assembly steps that go through..This value was the bus frequency not the ISCOUT..The clocks are like this, first the DCOOUT, then i want to divide by four to have a ISCOUT of 8MHz, and later the bus frequency is predefined as ISCOUT/2 and that will be 4MHz...I dont know if im doing a wrong configuration, please help me....I already have the 4MHz in the bus freq, but im afraid that i did a wrong configuration, because i changed the BDIV bitfields and the bus frequency did not work...

 

#define FTrim_Val 0
#define ICSC1_FEI 0b00000100
#define ICSC2_FEI 0b00010110      //Con los dos primeros cuadro ISCOUT division DCOOUT/1                                                //DCOOUT=8MHz y ISCOUT=4Mhz
#define ICSSC_FEI 0b01000000 | FTrim_Val     //Midrange DCO32Mhz,dmx32=0,,,,Ftrim Default 0

 

I did this changing the BDIV bitfields in the ICSC2 register first from 0b10 (DCOOUT/4) and later with 00 (DCOOUT/1)and the result was the same....a 4MHz MCU frequency...and the command box in the debugger tells me that the MCU speed is 4MHz...

 

Thanks, please help me...

标签 (1)
0 项奖励
回复
1 解答
2,310 次查看
RichTestardi
Senior Contributor II

Hi,

 

Maybe this will help...  I believe this sequence will output your bus frequency divided by ~1000 to pin ptc0:

 

                    TPM3SC = TPM3SC_CLKSA_MASK;
                    TPM3C0SC = TPM3C0SC_MS0A_MASK;
                    TPM3MODH = 499>>8;
                    TPM3MODL = 499&0xff;
                    TPM3CNTL = 0;
                    TPM3C0SC_ELS0x = 1;
                    TPM3C0VH = 499>>8;
                    TPM3C0VL = 499&0xff;

 

That's how I usually validate I have programmed my clocks correctly -- by dividing them down and sending them off-chip where I can measure them for sure.

 

I just ran the above code on my MCF51QE128 and saw 25kHz.

 

-- Rich

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,311 次查看
RichTestardi
Senior Contributor II

Hi,

 

Maybe this will help...  I believe this sequence will output your bus frequency divided by ~1000 to pin ptc0:

 

                    TPM3SC = TPM3SC_CLKSA_MASK;
                    TPM3C0SC = TPM3C0SC_MS0A_MASK;
                    TPM3MODH = 499>>8;
                    TPM3MODL = 499&0xff;
                    TPM3CNTL = 0;
                    TPM3C0SC_ELS0x = 1;
                    TPM3C0VH = 499>>8;
                    TPM3C0VL = 499&0xff;

 

That's how I usually validate I have programmed my clocks correctly -- by dividing them down and sending them off-chip where I can measure them for sure.

 

I just ran the above code on my MCF51QE128 and saw 25kHz.

 

-- Rich

0 项奖励
回复
2,310 次查看
jreyes085
Contributor I
Thanks!
0 项奖励
回复
2,310 次查看
guribe
Contributor I

Hi:

 

  The real questions is: Why may we go to ask through a Forum, such kind of technical data that MUST be in the manuals? Today, 3 years after Rich T's kind advise, I am here looking for the same data (what is THE FFFrequency of the thing), after hours of reading ALL reference manuals, ALL Quick start guides, ALL schematics, ALL User Guides, ALL C examples, ALL asm examples (only ONE...).

 

  Reversing engineering to find out technical details needed to design, is NOT what I am needing to do today.

 

Eng. Luis G. Uribe C.

0 项奖励
回复
2,310 次查看
guribe
Contributor I

And I am NOT a Newbie

0 项奖励
回复
2,310 次查看
iapetus
Contributor I

hehe i came across with the same matter when i was studying at university. Can i ask u a question? are u from Colombia? Xaverian university?

0 项奖励
回复
2,310 次查看
guribe
Contributor I

  YES! 38 años ahora en Caracas. USB primero, empleado luego en empresas de tecnología (Coasin, Autotrol), luego mías en sociedad (Vessing, VT&D, Electriahorro), retirado y... des-retirado después, a mis 65 años, gracias a mis socios! Y tu eres?

 

  Interesante tu observación! Saludos, GUribe (algo desactualizado: http://uribe.tk/ ...)

0 项奖励
回复