How to generate M52235 UART interrupt?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to generate M52235 UART interrupt?

4,029件の閲覧回数
ylkoh
Contributor I
Hi,
 Is there anybody can tell me how to generate UART0 interrupt?
 Currently, I can getchar/putchar from UART0 to Terminal already. But the problem is I am not able to generate an interrupt while Rx and Tx.
 Can somebody help me? it would be better to have an example.
 Thanks in advance.
 
 
Regards,
YL Koh
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,791件の閲覧回数
Nouchi
Senior Contributor II
hi,

1 - Install your ISR routine in exeption table :   /* see Chap 15.6.3.1 to know  source number */
__VECTOR_RAM[64+13] = (uint32)YourISRFunction; 
2 -  Program interrupt controller                     /* see Chap 15.3.6  &  15.3.2*/
   MCF_INTC_ICR(13) |= MCF_INTC_ICR_IL(3) | MCF_INTC_ICR_IP(3);   /* set It level & priority */
   MCF_INTC_IMRL &= ~(MCF_INTC_IMRL_MASK13 + MCF_INTC_IMRL_MASKALL);  /* enable it */
3 - enable uart interrupt                               /* see chap 26.3.1 & 26.3.10 */
   MCF_UART_UMR(0) = what you need;         /*select interrupt Fifo full or RXRDY */
   MCF_UART_UIMR(0) = MCF_UART_UIMR_RXRDY_FU + MCF_UART_UIMR_TXRDY; /* enable interrupts */
4 - in your ISR routine, check status register   /* see chap 26.3.3 */
   ucStatus = MCF_UART_USR(0);            /* read status register */
   and deal with status register flags (error flags FE, OE and PE and RXTX flags TXRDY, FFULL or RXRDY)


Emmanuel

0 件の賞賛
返信

1,791件の閲覧回数
ylkoh
Contributor I
Hi BugMan,
 
 Thanks for you reply.
 BTW, I still can't get any interrupt.
 I am using vector table to generate the ISR
 vector4D: .long _uart0_handler
 Here is what I wrote.
 
void
mcf52235_uart_init(void)
{
 /*
 * Initialize all three UARTs for serial communications
 */
 register uint16 ubgs;
 /*
 * Set Port UA to initialize URXD0/UTXD0
 */
   MCF_GPIO_PUAPAR = 0
       | MCF_GPIO_PUAPAR_RXD0_RXD0
       | MCF_GPIO_PUAPAR_TXD0_TXD0;
   MCF_GPIO_PUBPAR = 0
       | MCF_GPIO_PUBPAR_RXD1_RXD1
       | MCF_GPIO_PUBPAR_TXD1_TXD1;
   MCF_GPIO_PUCPAR = 0
       | MCF_GPIO_PUCPAR_RXD2_RXD2
       | MCF_GPIO_PUCPAR_TXD2_TXD2;
 /*
 * Reset Transmitter
 */
 MCF_UART0_UCR = MCF_UART_UCR_RESET_TX;
 MCF_UART1_UCR = MCF_UART_UCR_RESET_TX;
 MCF_UART2_UCR = MCF_UART_UCR_RESET_TX;
 /*
 * Reset Receiver
 */
 MCF_UART0_UCR = MCF_UART_UCR_RESET_RX;
 MCF_UART1_UCR = MCF_UART_UCR_RESET_RX;
 MCF_UART2_UCR = MCF_UART_UCR_RESET_RX;
 /*
 * Reset Mode Register
 */
 MCF_UART0_UCR = MCF_UART_UCR_RESET_MR;
 MCF_UART1_UCR = MCF_UART_UCR_RESET_MR;
 MCF_UART2_UCR = MCF_UART_UCR_RESET_MR;

 /*
 * No parity, 8-bits per character
 */
 MCF_UART0_UMR = (0
  | MCF_UART_UMR_RXIRQ
  | MCF_UART_UMR_RXRTS
  | MCF_UART_UMR_PM_NONE
  | MCF_UART_UMR_BC_8 );
 MCF_UART1_UMR = (0
  | MCF_UART_UMR_RXIRQ
  | MCF_UART_UMR_RXRTS
  | MCF_UART_UMR_PM_NONE
  | MCF_UART_UMR_BC_8 );
 MCF_UART2_UMR = (0
  | MCF_UART_UMR_PM_NONE
  | MCF_UART_UMR_BC_8 );
 /*
 * No echo or loopback, 1 stop bit
 */
 MCF_UART0_UMR = (0
  | MCF_UART_UMR_CM_NORMAL
  | MCF_UART_UMR_SB_STOP_BITS_1);
 MCF_UART1_UMR = (0
  | MCF_UART_UMR_CM_NORMAL
  | MCF_UART_UMR_SB_STOP_BITS_1);
 MCF_UART2_UMR = (0
  | MCF_UART_UMR_CM_NORMAL
  | MCF_UART_UMR_SB_STOP_BITS_1);
 /*
 * Set Rx and Tx baud by SYSTEM CLOCK
 */
 MCF_UART0_UCSR = (0
  | MCF_UART_UCSR_RCS_SYS_CLK
  | MCF_UART_UCSR_TCS_SYS_CLK);
 MCF_UART1_UCSR = (0
  | MCF_UART_UCSR_RCS_SYS_CLK
  | MCF_UART_UCSR_TCS_SYS_CLK);
 MCF_UART2_UCSR = (0
  | MCF_UART_UCSR_RCS_SYS_CLK
  | MCF_UART_UCSR_TCS_SYS_CLK);
 /*
 * Mask all UART interrupts
 */
 uart0_interrupt_init(); // added by ylkoh
 uart1_interrupt_init();
 //MCF_UART0_UIMR = 0;
 //MCF_UART1_UIMR = 0;
 MCF_UART2_UIMR = 0;
 
 /*
 * Calculate baud settings
 */
 ubgs = (uint16)((SYSTEM_CLOCK*1000000)/(UART_BAUD * 32));
 MCF_UART0_UBG1 = (uint8)((ubgs & 0xFF00) >> 8);
 MCF_UART0_UBG2 = (uint8)(ubgs & 0x00FF);
 MCF_UART1_UBG1 = (uint8)((ubgs & 0xFF00) >> 8);
 MCF_UART1_UBG2 = (uint8)(ubgs & 0x00FF);
 MCF_UART2_UBG1 = (uint8)((ubgs & 0xFF00) >> 8);
 MCF_UART2_UBG2 = (uint8)(ubgs & 0x00FF);
 /*
 * Enable receiver and transmitter
 */
 MCF_UART0_UCR = (0
  | MCF_UART_UCR_TX_ENABLED
  | MCF_UART_UCR_RX_ENABLED);
 MCF_UART1_UCR = (0
  | MCF_UART_UCR_TX_ENABLED
  | MCF_UART_UCR_RX_ENABLED);
 MCF_UART2_UCR = (0
  | MCF_UART_UCR_TX_ENABLED
  | MCF_UART_UCR_RX_ENABLED);
}
/********************************************************************/
// this function was added by ylkoh
void
uart0_interrupt_init(void)
{
 MCF_INTC1_ICR13 |= 0x3F;      // 111 111 => IL + IP
            // (Interrupt level + Interrupt priority)
 MCF_INTC0_IMRL &= ~(MCF_INTC_IMRL_MASK13 + MCF_INTC_IMRL_MASKALL); // refer to UM Interrupt Sources ch.15.3.6.1
 
 MCF_UART0_UIMR |= (0
     | MCF_UART_UIMR_TXRDY
     | MCF_UART_UIMR_RXRDY_FU);
     //| MCF_UART_UIMR_DB
     //| MCF_UART_UIMR_COS);
  
}
void
uart1_interrupt_init(void)
{
 MCF_INTC1_ICR14 |= 0x3F;      // 111 111 => IL + IP
            // (Interrupt level + Interrupt priority)
 MCF_INTC0_IMRL &= ~(MCF_INTC_IMRL_MASK13 + MCF_INTC_IMRL_MASKALL); // refer to UM Interrupt Sources ch.15.3.6.1
 
 MCF_UART1_UIMR |= (0
     | MCF_UART_UIMR_TXRDY
     | MCF_UART_UIMR_RXRDY_FU);
     //| MCF_UART_UIMR_DB
     //| MCF_UART_UIMR_COS);
  
}
 
 Can you help me find out what happen?
 Thanks in advance.
 
 
Regards,
YL Koh
0 件の賞賛
返信

1,791件の閲覧回数
Nouchi
Senior Contributor II
hello YL Koh,

Did you think to enable interrupts by setting the right level (usally to 0) to the 'I' field in SR CPU core register ?

Emmanuel
0 件の賞賛
返信