How to debug on my K64F on IAR using windows in a virtual machine?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to debug on my K64F on IAR using windows in a virtual machine?

1,219 Views
bayrammidassi
Contributor I

Hallo,

i have a problem to debug my Program which is developed on IAR using CMSIS/DAP on windows.

I am using Linux mate as the main OS and Windows in the virtual machine.

The problem is that windows does't detect the USB interface of my card K64F.

I added the card like a shared disc to my virtual machine but it does't work.

 

Any help?

thanks in advance

Labels (1)
0 Kudos
Reply
1 Reply

1,132 Views
miduo
NXP Employee
NXP Employee

Hi,

Have you tried the Vmware? From what I know the best way to run a virtual machine with real hardware is to use VMware and run a virtual XP session... it should works good with all sorts of USB drivers that seem to have trouble on win 7 and other virtual machines.. Be warned that VMware must take over exclusive use of the USB ports while running..

0 Kudos
Reply