Hi,  I'm using microcontroller Coldfire MCF52258CAG66 and IDE Code Warrior Version 5.9.0. I would like to know how much ROM & RAM I'm utizilizing in my application. Here is the map file:  ------------------------------------------------------------- # Mem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi,  I'm using microcontroller Coldfire MCF52258CAG66 and IDE Code Warrior Version 5.9.0. I would like to know how much ROM & RAM I'm utizilizing in my application. Here is the map file:  ------------------------------------------------------------- # Mem

1,379件の閲覧回数
mubashirazhar
Contributor I

Hi,

 

I'm using microcontroller Coldfire MCF52258CAG66 and IDE Code Warrior Version 5.9.0.

I would like to know how much ROM & RAM I'm utizilizing in my application.

Here is the map file:

 

-------------------------------------------------------------

# Memory map:

  v_addr   p_addr   size     name

  00006100 00006100 00000400 .vectors   vectorrom

  00006500 00006500 0005E518 .main_application rom

  0007FFFC 0007FFFC 00000004 .flashprot endflashrom

  20000000 00064A18 000009E4 .main_application_data ram

  200009E4 200009E4 00003868 .main_application_bss ram

  2000424C 2000424C 00000000 .kernel_data ram

  2000FFF0 2000FFF0 00000000 .end_of_kernel_data end_of_kd

  2000FA00 2000FA00 00000000 .boot_stack bstack

  2000FBFC 2000FBFC 00000000 .end_of_boot_stack end_bstack

  2000FBFC 000653FC 00000018 .romp      end_bstack

--------------------------------------------------------------

 

Also let me know if there is a feature in codewarrior to check RAM usage.

 

Thank you,

Mubashir

ラベル(1)
0 件の賞賛
返信
1 返信

1,178件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

From the memory file you attached, it seems that ROM is from 6100 to 65414 and the RAM is from 20000000 to 2000424C

You should add p_addr and size in the file to get the count.

PS: the address before 0x20000000 is ROM.

0 件の賞賛
返信