Hi, I have a problem when I tried to convert the data typ...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hi, I have a problem when I tried to convert the data typ...

4,746 次查看
xren
Contributor II
Hi, I have a problem when I tried to convert the data type. the processor is MCF5235CVM150 and the compiler is diab 5.2 from windriver (vxworks5.5.1). I have written a very simple function to test the type conversion. But the results were not as expected.

void typwad()
{
    float fv = 2147470000.0;/*2147483646.0;*/
    int iv;
   
    printf("sizeof(float) = %d, fv = %f\n",sizeof(fv),fv);

    iv = (int)fv;
    printf("int iv = %d\n", iv);

    return;
}

and the results are:
sizeof(float) = 4, fv = 2147469952.000000
int iv = 2147469952

when I changed the fv value to 2147483646.0, the results are:
sizeof(float) = 4, fv = 2147483648.000000
int iv = -2147483648

I don't understand whether this is a precision problem or something else caused by compiler.  I really appreciate it if somebody can give me a hint.

I paste also the dissembled code here just for convenience.
void typwad()
{
    0x209330       _typwad:                LINK  .W    A6,#0xfff8
    0x209334       +0x004:                 MOVE  .L    D7,-(A7)
    float fv = 2147470000.0;/*2147483646.0;*/
    0x209336       +0x006:                 MOVE  .L    #0x4effff95,D0
    0x20933c       +0x00c:                 MOVE  .L    D0,(0xfffc,A6)
    int iv;
   
    printf("sizeof(float) = %d, fv = %f\n",sizeof(fv),fv);
    0x209340       +0x010:                 MOVE  .L    (0xfffc,A6),D0
    0x209344       +0x014:                 JSR         fltodb
    0x20934a       +0x01a:                 MOVE  .L    D1,-(A7)
    0x20934c       +0x01c:                 MOVE  .L    D0,-(A7)
    0x20934e       +0x01e:                 MOVEQ       #0x4,D0
    0x209350       +0x020:                 MOVE  .L    D0,-(A7)
    0x209352       +0x022:                 PEA         _str_cmp + 0xca
    0x209358       +0x028:                 JSR         _printf
    0x20935e       +0x02e:                 LEA         (0x10,A7),A7

    iv = (int)fv;
    0x209362       +0x032:                 MOVE  .L    (0xfffc,A6),D0
    0x209366       +0x036:                 JSR         fltol
    0x20936c       +0x03c:                 MOVE  .L    D0,D7
    printf("int iv = %d\n", iv);
    0x20936e       +0x03e:                 MOVE  .L    D7,-(A7)
    0x209370       +0x040:                 PEA         _str_cmp + 0xe7
    0x209376       +0x046:                 JSR         _printf
    0x20937c       +0x04c:                 ADDQ  .L    #0x8,A7

    return;
}
    0x20937e       +0x04e:                 MOVE  .L    (0xfff4,A6),D7
    0x209382       +0x052:                 UNLK        A6
    0x209384       +0x054:                 RTS        
    0x209386       +0x056:                 NOP        



标签 (1)
6 回复数

3,512 次查看
xren
Contributor II
Hi, Rich.

But what I don't understand is why the printed float value is also not correct. 

The float variable fv has been asigned 2147470000.0, which does not exceed the limit.

when I printed it on the console using printf("sizeof(float) = %d, fv = %f\n",sizeof(fv),fv); the result is
fv = 2147469952.000000

0 项奖励
回复

3,512 次查看
RichTestardi
Senior Contributor II
Hi,
 
The issue is the rounding you can't really avoid.  Not only can (most) integer numbers not be represented exactly in a 32 bit floating point value, also most *real* numbers cannot be represented, either.  Consider your number:
 
  2147470000.00
 
This is converted to 32 bit floating point as:
 
  4EFFFF95
 
Which is:
 
  +1 .11111111111111110010101 x 2^30
 
If you look at the floating point numbers in this area (the density of floating point numbers is not uniform), you will see:
 
  4EFFFF94 = 2147469824.00
  4EFFFF95 = 2147469952.00
  4EFFFF96 = 2147470080.00
 
So you can see that for the number you requested (2147470000.00) the compiler had to choose the nearest floating point value (based on its rounding algorithm), and it chose 4EFFFF95.  But once you tried to print it back out, it no longer knew what you requested -- only the real number -- so it printed it out exactly as 2147469952.00.
 
 There are floating point calculators on the web which allow you to do this, such as:
 
 
-- Rich
 

3,512 次查看
RichTestardi
Senior Contributor II
Oh, and I'll add one more link:
 
 
That might clear things up, as well.
0 项奖励
回复

3,512 次查看
xren
Contributor II
Thanks a lot, Rich. Now it is quite clear.
0 项奖励
回复

3,512 次查看
RichTestardi
Senior Contributor II
Hi,
 
I might not understand exactly what problem you are having, and which behavior you don't like...
 
A 4 byte float has less than 4 bytes for the mantissa, so it can't represent (most) 4 byte integers exactly, so rounding (up or down) occurs.
 
And when you convert from float to back to integer, the floating point value may not be representable in the integer's width at all.
 
(In your second case, you would have needed a 33 bit signed integer to represent the value.  A 32 bit signed integer can represent the values from +2^31-1 to -2^31.  If you had used an unsigned integer there (and a %u) you probably would have been OK, but you still would have had the rounding in the floating point value.)
 
-- Rich
0 项奖励
回复

3,512 次查看
xren
Contributor II
Thank you so much, rich.  Now I understand what the problem is.

According to C specification, the four bytes single float format is

                    Address+0        Address+1        Address+2       Address+3

Contents   SEEE EEEE       EMMM MMMM   MMMM MMMM    MMMM MMMM


S is the sign bit, Es are exponent part and Ms are mantissa part. For a single float, the effective bits number is 24 while an integer has 32.
0 项奖励
回复