Help setting up interrupr driven UART on 52223

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help setting up interrupr driven UART on 52223

2,007 Views
PopsStack
Contributor I
Can someone please assist with setting up interrupt driven UART.
 
I see that reference is made to the CTS line being sensed for interrupt t oocurr or am I missing something here. I am not using CTS only RX,TX, GND lines.
 
Am try to get data out of a GPS so need to get the data out and stash it in a buffer to then parse it for the NMEA sentences.
 
Thanks
 
PS
Labels (1)
0 Kudos
Reply
1 Reply

1,192 Views
mjbcswitzerland
Specialist V
Hi PS

The RTS + CTS are not needed and can be ignored.

See the following:
http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&thread.id=4196
the M52223 UARTs are compatible to the M5223X and code is identical.

Regards

Mark

www.uTasker.com

0 Kudos
Reply