Help QADC from coldfire 5282

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help QADC from coldfire 5282

1,807 Views
Lucho
Contributor I
I'm tring to use the module QADC from the coldfire 5282. I have problems with the registers of this QADC, I configure it for AN0 and I send the answer to the port TC and I don't have eny answer. If someone have an exemple of this please send it to me.
Labels (1)
0 Kudos
Reply
1 Reply

1,189 Views
PaoloRenzo
Contributor V

Lucho wrote:
I'm tring to use the module QADC from the coldfire 5282. I have problems with the registers of this QADC, I configure it for AN0 and I send the answer to the port TC and I don't have eny answer. If someone have an exemple of this please send it to me.


Hi:



Maybe you are using interrupts and using a stationary code from Codewarrior.

By default, vector table is not included in RAM target, only in ROM targets, so if you are using debug green arrow, is not enough.

In order to allow interrupts you have to burn FLASH memory to include the vector table (vector.s). After that you can debug the code, but, as I said, only in ROM targets.

Only guessing your problem :smileywink:

Good luck!
0 Kudos
Reply