[Help!] Demo of EKG recording

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Help!] Demo of EKG recording

1,155 Views
bonbonking
Contributor I
Hi Everybody, I'm a computer science student who is currently working on a EKG authentication project. Now i'm using TWR-MCF51MM-KIT (which is a medical-oriented development tool for the MCF51MM256 microcontroller ) (http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF51MM) and a Medical EKG board ( http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MED-EKG&fsrch=1&sr=13 ) as my device to collect EKG from different people. I've just got started and I've succeed in running a EKG Lab on CodeWarrior v6.3 with a MED-EKG GUI. But my main challenge is to collect these EKG data from the device. I have several rough ideas, like I should use USB PHDC to retrieve data and then process them. But I'm really lost right now. Can anyone give me some ideas about where to start and how? Many thanks in advance!!
Labels (1)
0 Kudos
Reply
3 Replies

964 Views
Jarrarist
Contributor I

Hey, I'm in your same situation, although I think I'm a step behind,

 

I've programmed the kit to run LAB1, and whether I use the on-board electrodes or an external electrode, I get a signal that's only fluctuating between -16000 and -13000, 

 

Sometimes it fluctuates also between that range and 0

 

You can see the pictures

 

 

0 Kudos
Reply

964 Views
Jarrarist
Contributor I

I meant those pictures

0 Kudos
Reply

964 Views
bonbonking
Contributor I
"Previous sections have mentioned that the GUI communicates with the microco ntroller via USB port, using the Freescale USB stack, which performs an algorithm that creates a virtual serial port to send and receive data"
I've noticed this from a tutorial...don't know if this bring some information......
0 Kudos
Reply