HCS12 source implementation into ColdFire

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCS12 source implementation into ColdFire

1,799 Views
BoSCHoW
Contributor II
Hello,

i was recently working with motorola microprocessor HCS12. Now i
decided to try a stronger microcontroller ColdFire and i dont wan't to
write the whole code all over again. So i am asking you how to
implement the existing code written for HCS12 to ColdFire
microcontroller ?

Thanks and best regards.


Message Edited by BoSCHoW on 2008-02-07 04:46 PM
Labels (1)
0 Kudos
Reply
1 Reply

1,101 Views
RickN
Contributor I
Hi,
 
   Is your HCS12 code written in the C programming language? 
 
    You are in for a decent amount of work to port your application code.  You will have a different memory map, and the registers will be different.   The peripherals will also need to be revisited, as the basic functionality may be similar (ADC, Timer, ...) but the registers will most likely be different.   If you have application code, written in C, that does not deal with any registers, it may port pretty cleanly if you make sure the data type sizes match.  On the upside, you have a flat memory model with 32 bit address space and 32 bit data bus on the ColdFire V2, V3 & V4 processors. 
 
    There are some tools available in CodeWarrior which can help generate code for your project.  A rapid application development tool called Processor Expert is included with CodeWarrior for ColdFire v7.0, and can generate C code for many of the processors in the ColdFire family. 
 
   Thanks,
 
   Rick
0 Kudos
Reply