General signal generation using data buffer fed with DMA transfers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

General signal generation using data buffer fed with DMA transfers

1,037件の閲覧回数
javiercambra
Contributor II

Hello,

 

 

 

I am trying to feed the DAC buffer using the DMA. We can find a simple example in the  DAC_LDD help.

 

 

 

I configured the devices following this example step by step, but does not work. The execution thread never reach the event DA1_OnComplete.

 

 

 

When configuring the DAC_LDD device in processor expert you can see that "Hardware trigger" must be Enable. But no more details are explained in this example. If I enable "Hardware trigger", then only can choose PDB, but in this example does not appear anything related to PDB, so I am little confused, and I don't know how to configure the trigger.


Any help will be apreciated.

 

I am using the microcontroller ColdFire V1+ MCF51QM128VLH and CodeWarrior 10.2

 

Regards,

Javi

 

 

 

 

 

ラベル(1)
タグ(3)
0 件の賞賛
返信
0 返答(返信)