GNU tools for M52233DEMO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GNU tools for M52233DEMO

4,889 Views
idon
Contributor I
Hi all,

We just got this dev board in a few weeks ago. It came with a CD which had a cygwin distribution on it, but all the files appear to be for the 5282. Will this also work for the 52233?

I was also looking at another GNU toolchain from Code-sourcery (whose link i found in this very forum). Would we be able to build with Sourcery G++ for uCLinux (or for ELF) as well? Which CPU type would I specify? I saw a posting here that 5208 worked.

And lastly, can we use either of these to build uCLinux for this Coldfire?

Hope you can help a newbie out.
Don
Labels (1)
0 Kudos
Reply
2 Replies

1,479 Views
admin
Specialist II
Hello,

I am using the M5223EVB with a MCF52235.

Here is a link to set up a GNU toolchain for the ColdFire:
http://www.cambridgeimaging.co.uk/wp_open-source-coldfire-ide.php

I wrote the hardware initialisation using the CFInit-Tool:
http://www.microapl.co.uk/CFInit/cfinit_main.html

I successfully managed to get the program debugged when run in RAM. I am currently working on debugging from ROM. I hope to find out about it soon.

Hope that helps.

Best regards
Nathan
0 Kudos
Reply

1,479 Views
Alban
Senior Contributor II
Hi Nathan,

Many thanks for these links.
I put this thread as "sticky" at the top of the list as I am sure developpers will appreciate this first participation of yours! :smileyhappy:

Welcome.
Alban.
0 Kudos
Reply