Flashing problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flashing problem

3,593 次查看
sirlenzelot
Contributor II
Hi Folks,
I am looking for tool that can upload my software to the onboard Flash like CF-Flasher.
But I can't use the Parallel or USB P&E Interface. I am using the Abatron BDI2000.
Can someone give me a hint, please?
 
Thanks
 
best regards
Dirk
 
标签 (1)
0 项奖励
回复
4 回复数

2,454 次查看
mwaddel
Contributor I
What platform are you using?
0 项奖励
回复

2,454 次查看
sirlenzelot
Contributor II
I am using Windows XP SP3.
Maybe I can install cygwin. I have to talk to my boss.
0 项奖励
回复

2,454 次查看
mwaddel
Contributor I
I should have been more specific.  I meant what target are you
using?  Abatron already has Coldfire support for a lot of targets:

mcf5206.cfg    mcf5213.cfg  mcf5272.cfg  mcf5329.cfg  mcf5485_mmu.cfg
mcf5206e.cfg  mcf5249.cfg  mcf5282.cfg  mcf5407.cfg
mcf5208.cfg    mcf5271.cfg  mcf5307.cfg  mcf5485.cfg

I use the bdi2000 to write to flash on some of the newer targets
also:

mcf52277.cfg  mcf5253.cfg  mcf5373.cfg

Is your bdi setup for a Coldfire target?  If it is, then your need
to copy the correct config file and register file to a tftp exported
directory.  The manual that came with the bdi device has
instructions to do this.  There are also instructions for reading,
writing and erasing flash.
0 项奖励
回复

2,454 次查看
sirlenzelot
Contributor II
Hi again,
 
I'm using the MCF5234. A config-file exists and is loaded to the BDI via the BDI-Tool.
Via Telnet i can set the Flash to write-mode.
But I am missing something to transfer the file from my PC to the FLASH.
 
In my manual (V1.00)  I can't find anything for transfering data to the FLASH.
There is something on Section 5, but I don't have any IDE (like EDGE/ECLIPSE) or else on the PC which needs to flash my boards. So I am looking for a standalone solution.
 
Thanks a lot
 
vy 73
Dirk
0 项奖励
回复