Flashing a MCF52233 in-system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing a MCF52233 in-system

1,311 Views
ZeroOne
Contributor I
Hello

I have a M52233DEMO board and I am considering to create my own board for a project I have in mind.
Is it possible to flash a new board with a MCF52233 onbord, in-system so to speak?

If yes, how?

Regards

Kim

Labels (1)
0 Kudos
Reply
1 Reply

648 Views
mjbcswitzerland
Specialist V
Hi

See the following: http://www.utasker.com/forum/index.php?topic=77.0

If you only want to FLASH programs (and not debug) the EZport offers the simplest connection - code running on the M52233DEMO can also do this - see: http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=3911&query.id=30163#M...

Regards

Mark

0 Kudos
Reply