Flash read/write help with the MCF52233 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash read/write help with the MCF52233 board

1,680件の閲覧回数
Motti
Contributor I

Hi,

 

I've developed a project based off the Coldfire_lite TCP project.  I'm using TCP on multiple boards to communicate with a server.  The TCP program works well as well as the other tasks I've created on the RTOS.  The only thing left is to create a menu option using the console that would allow a user to change the IP address and other network related info so that the boards don't create any conflicts on the LAN.

 

I am trying to create a function that would take in the new IP from the uart and flash it to a safe place in FLASH memory.  I don't fully understand the commands used to both read and write to flash from the embedded software and I don't want to store the address in RAM (I've done that already).

 

If anybody has any experience with this and could guide me where to look I would really appreciate the help.

 

Thanks.

 

Motti

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,211件の閲覧回数
mjbcswitzerland
Specialist V

Hi Motti

 

See: http://www.utasker.com/docs/uTasker/uTaskerFileSystem_3.PDF (section about parameter system).

 

Regards

 

Mark

 

www.uTasker.com

 

 

0 件の賞賛
返信

1,211件の閲覧回数
Motti
Contributor I

Hi Mark,

 

Thanks for the link.  It's just what i was looking for.  I'll check out the demo code in uTasker.

 

Motti

0 件の賞賛
返信