Flash Problem 52235

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Problem 52235

1,931 Views
Frank13
Contributor I

Hi!

 

I just wanted to start with my cobra52235-board. I use the 52235EVB test example from codewarrior. The program runs from RAM, but when I program it to Flash and try to debug, I get the following error. I use the CobraConnect Interface (compatible to P&E parallel interface).

 

Greetings

 

Frank Bußmann

 

Exception vector name: Bus ErrorPC where the exception happened: 0x00000A5Cthe code there is:
/* *    Startup routine for embedded application ... */asm void __declspec(register_abi) _startup(void){    /* disable interrupts */    move.w        #0x2700,sr.....
Labels (1)
0 Kudos
Reply
2 Replies

1,482 Views
TomE
Specialist II

Dump (examine memory before, at and after) 0x00000A5C and see what it decodes to.

 

Disassemble it using the debugger and then cross-check by hand-disassembling it as well.

 

Dump the whole vector area (from zero) and ensure the initial PC and SP are sane (and pointing to the above).

 

Can you single-step it from reset and see where it goes?

 

Internal or external FLASH?

 

 

0 Kudos
Reply

1,482 Views
Frank13
Contributor I

Hi!

 

It must have been a problem within the codewarrior. Today morning I tried again and got some different errors. A reinstallation of the compiler solved the problem.

 

Thanks!

 

Greetings

 

Frank

0 Kudos
Reply