Field upgrade firmware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Field upgrade firmware

ソリューションへジャンプ
3,097件の閲覧回数
mstone59
Contributor II
Hello,
 
I'm relatively new to embedded programming. I've worked on a project that uses a MCF5213, I was told yesterday that I need to make the firmware field upgradable. The only current interface I have is RS485 through one of the uarts. It would be great to find an example implementation for this micro, but even pointing me to a good book would be great. Please help, I have to be done by January 20th, 2008.
 
Thank you.
ラベル(1)
0 件の賞賛
返信
1 解決策
1,763件の閲覧回数
mstone59
Contributor II
Thank you for the feedback. I was able to convince my supervisor that this feature should be added to the next revision of software. I am starting my research on it now.
 
Thank you,
Mike

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,763件の閲覧回数
SimonMarsden_de
Contributor II
Hi

A good place to start might be to look at the source code of the dBUG application. This is the resident monitor which comes with the Freescale evaluation boards. It would show you how to reprogram the Flash on the MCF5213, and how to bring the chip up and configure a serial port. You'd still need to do a fair amount of work, but it might be a useful resource.

The dBUG source should be downloadable from Freescale's web site.

Hope this helps


Simon
0 件の賞賛
返信
1,764件の閲覧回数
mstone59
Contributor II
Thank you for the feedback. I was able to convince my supervisor that this feature should be added to the next revision of software. I am starting my research on it now.
 
Thank you,
Mike
0 件の賞賛
返信