Fast Ethernet Drivers  (FEC) for MCF5235EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fast Ethernet Drivers  (FEC) for MCF5235EVB

Jump to solution
1,701 Views
kolett999
Contributor I

Where can I find the Ethernet drivers for the MCF5235EVB ?

Or also find some source code  that could be used  like example ?

 

many thanks.

 

stephen

Labels (1)
0 Kudos
Reply
1 Solution
1,591 Views
Nouchi
Senior Contributor II

Hello,

You could have a look to fnet and the MCF5282 port, which is close to the MCF5235.

An alternative solution is FreeRTOS with the lwIP_MCF5235_GCC demo, or RTEMS, a very mature system with MCF5235EVB bsp

Emmanuel

View solution in original post

0 Kudos
Reply
1 Reply
1,592 Views
Nouchi
Senior Contributor II

Hello,

You could have a look to fnet and the MCF5282 port, which is close to the MCF5235.

An alternative solution is FreeRTOS with the lwIP_MCF5235_GCC demo, or RTEMS, a very mature system with MCF5235EVB bsp

Emmanuel

0 Kudos
Reply