Extremely hot Coldfire in Zoom kit.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Extremely hot Coldfire in Zoom kit.

3,067件の閲覧回数
peddamat
Contributor I
Hi everyone,

I just got my hands on a shiny, new Zoom dev kit and noticed the Coldfire processor gets very, very hot. Hot enough that I'm worried about inserting a CF card in the CF adaptor, lest I melt the card and the board. How hot is the processor supposed to get?

Other than the heat, the kit is great.



Sumanth Peddamatham
ラベル(1)
0 件の賞賛
返信
1 返信

1,236件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Sumanth,

He are some engineering power numbers....yes it runs hot.

The following numbers where measured on a MCF5475 running at 66/132/264 MHz at room temperature.

 

Instructions in Flash (Flexbus, 3.3V IO)
Data in external SRAM (Flexbus, 3.3V IO)
SDRAM drive turned on to 8mA drive strength

Caches on

DMA moving data from external SRAM to FEC FIFO
FEC continually transmitting data at 10Mbps / half-duplex
CPU alternates reads of SDRAM and internal registers
---------------------------------
1.48V Core     557 mA    .824W
2.50V DDR      227 mA    .568W
3.27V uP I/O    31 mA    .101W
                       ---------
                        1.493W

 

 

Note these are only the power measurements for the voltage rails into the processor.  The external memory power budgets are not accounted for here.

I can tell you that the non-encryption parts require ~135mA less on the 1.5V power supply; This saves about 200 mWatts.

Regards, David

0 件の賞賛
返信