External SRAM interface with 5328

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External SRAM interface with 5328

2,870 Views
Soos
Contributor III
I want to interface external 16-bit SRAM & 16-bit FLASH to 5328. I got confused because of split bus mode setting & not sure whether I should connect D0-D15 or D16-D31. I am not using any other type of RAM.
Can anybody help me in this regard ?
Thanks in advance.

Labels (1)
0 Kudos
Reply
2 Replies

1,771 Views
obidon
Contributor III
0 Kudos
Reply

1,771 Views
Soos
Contributor III
Thanks Obidon,
This PDF is realy useful.
- Soos
0 Kudos
Reply