Ethernet Rx interrupt handling in FNET Stack

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet Rx interrupt handling in FNET Stack

1,579 Views
Neerajjaini
Contributor I

Hello,

 

We are using FNET Stack for MCF52259 based application.

 

Some information is required to optimize my application, I need to clarify following.

 

1.) Multiple Ethernet RX buffer and Tx Buffer are used. Why it is required and its benefit?

2.) After doing some brief study of FNET stack,it appears that after receiving the Ethernet Frame some software interrupt is generated for ARP and IP.

 

Please know me , How software interrupt is executing while Vector number of SW interrupts are  out of Vector table  or  there is other mechanism used  to  slice f Ethernet Receive frame interrupt.

Labels (1)
0 Kudos
Reply
1 Reply

1,280 Views
butok
NXP Employee
NXP Employee

Hi Neerajjaini,

 

>>Multiple Ethernet RX buffer and Tx Buffer are used. Why it is required and its benefit?


It is enough to have two TX buffers (defined by FNET_CFG_CPU_ETH_TX_BUFS_MAX). While FEC sends frame from one buffer, the FEC driver may fill the second one.

On practice, two RX buffers can be enough (defined by FNET_CFG_CPU_ETH_RX_BUFS_MAX), but you can set it to bigger value to avoid dropping of received frames if an application is not so fast to handle them on time.

 

>>2.) after receiving the Ethernet Frame some software interrupt is generated for ARP and IP.


These “SW interrupts” are not  "real" interrupts. They are functions that use functionality of the FNET Interrupt Scheduler and critical code blocking mechanism.

 

>>How software interrupt is executing while Vector number of SW interrupts


They are not registered in CPU vector table (as they are not connected to HW), they are called by SW.

 

 

BTW: You can send any FNET improvements/fixes (if any) directly to [email protected]


Thank you,

Andrey Butok

0 Kudos
Reply