Errors on CODE WARRIOR headers Files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Errors on CODE WARRIOR headers Files

2,083件の閲覧回数
p_vagnoni
Contributor III
Hello all,
 
Working with the Code Warrior for the MCF52235 I find errors on the header file GPIO.H.
 
I listed this errors in another Thread but I have no reply in last 2 days. Is there someone in FREESCALE that is working on this bugs? It isn't my job but I hve to check or rewrite myself all headers file to start working better with this micro?
My check is complete on gpio.h file, I have only some question before attached in this thread:
 
In some ports we have up to 4 functionality for each pin, as described in Table 2-1 of the Reference Manual. In the bit definition for this register (PxxPAR) there are no mention on some of them. one example is:
 
Code:
/* Bit definitions and macros for MCF_GPIO_PNQPAR */#define MCF_GPIO_PNQPAR_PNQPAR1(x)     (((x)&0x0003)<<2)#define MCF_GPIO_PNQPAR_PNQPAR2(x)     (((x)&0x0003)<<4)#define MCF_GPIO_PNQPAR_PNQPAR3(x)     (((x)&0x0003)<<6)#define MCF_GPIO_PNQPAR_PNQPAR4(x)     (((x)&0x0003)<<8)#define MCF_GPIO_PNQPAR_PNQPAR5(x)     (((x)&0x0003)<<10)#define MCF_GPIO_PNQPAR_PNQPAR6(x)     (((x)&0x0003)<<12)#define MCF_GPIO_PNQPAR_PNQPAR7(x)     (((x)&0x0003)<<14)#define MCF_GPIO_PNQPAR_IRQ1_GPIO      (0x0000)#define MCF_GPIO_PNQPAR_IRQ2_GPIO      (0x0000)#define MCF_GPIO_PNQPAR_IRQ3_GPIO      (0x0000)#define MCF_GPIO_PNQPAR_IRQ4_GPIO      (0x0000)#define MCF_GPIO_PNQPAR_IRQ5_GPIO      (0x0000)#define MCF_GPIO_PNQPAR_IRQ6_GPIO      (0x0000)#define MCF_GPIO_PNQPAR_IRQ7_GPIO      (0x0000)#define MCF_GPIO_PNQPAR_IRQ1_IRQ1      (0x0004)#define MCF_GPIO_PNQPAR_IRQ2_IRQ2      (0x0010)#define MCF_GPIO_PNQPAR_IRQ3_IRQ3      (0x0040)#define MCF_GPIO_PNQPAR_IRQ4_IRQ4      (0x0100)#define MCF_GPIO_PNQPAR_IRQ5_IRQ5      (0x0400)#define MCF_GPIO_PNQPAR_IRQ6_IRQ6      (0x1000)#define MCF_GPIO_PNQPAR_IRQ7_IRQ7      (0x4000)#define MCF_GPIO_PNQPAR_IRQ1_SYNCA     (0x0008)#define MCF_GPIO_PNQPAR_IRQ1_PWM1      (0x000C)

Note that the last 2 rows are corrected because were wrong (were 0x8000 and 0xC000).
 
In table 2-1 I read that it could be respectively:
 
PRIMARY SECONDARY TERTIARY   QUATERNARY
 
IRQ2    ---       FEC_RXD[3] PNQ[2]
IRQ3    ---       FEC_RXD[2] PNQ[3]
IRQ5    ---       FEC_RXD[1] PNQ[5]
IRQ6    ---       FEC_RXER   PNQ[6]

My question is: where are the Tertiary function definition for pins 2, 3, 5, and 6 ?
 
Note that this is also true for other QUAD FUNCTION PIN ASSIGNMENT REGISTER.
 
Thanks
ラベル(1)
0 件の賞賛
返信
1 返信

1,157件の閲覧回数
Alban
Senior Contributor II
Hello Paolo,

The Official Freescale Support does not get assignments from the Forums.
To be certain to get involvment from Freescale Support Representative, you need to submit a Service Request.

POST: [Important] How to get Technical Support

I also advise all members/visitors to have a look at the

BOARD: Forum Use, Policies, and General Questions
Post questions about the forum itself there. Share your tricks. Suggest improvements and give your feedback to the admins. All other General questions are welcomed.
Please NO technical question on this board, they will be moved or simply deleted.



Cheers,
Alban.
0 件の賞賛
返信