Error on LTIB Install

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error on LTIB Install

2,230件の閲覧回数
Dome
Contributor II
Hi

We have just purchased a EVBMCF5329 but we have a problem whit ./ltib, it come out whit this error:

+ umask 022
+ cd /tmp/rpm-nik/BUILD
+ cd rpm-4.0.4
+ set +e
++ ls /lib/tls/libc-2.3.5.so /lib/tls/libc-2.3.6.so
+ HAS_TLS_LIBC='/lib/tls/libc-2.3.5.so
/lib/tls/libc-2.3.6.so'
+ set -e
+ '[' -n '/lib/tls/libc-2.3.5.so
/lib/tls/libc-2.3.6.so' ']'
+ MIN_LIBC_VER=2.2.5
+ export LD_ASSUME_KERNEL=2.2.5
+ LD_ASSUME_KERNEL=2.2.5
++ echo /opt/freescale/ltib/usr
++ sed -e 's,/usr$,,'
sed: error while loading shared libraries: libc.so.6: cannot open shared object file: No such file or directory
+ var=/var
error: Bad exit status from /tmp/rpm-tmp.23386 (%build)

But i have all required library (libc.so.6) and binary!

We also downloaded the latest uClinux distribution but we don't achive to compile it because the freescale toolchain don't work, asm error, and we are tryng to donwload the latest official uclinux-tools (20060615) but it's very very slow (1k/s).

Somebody can give me a usefull tip?

Thanks, Dome
ラベル(1)
0 件の賞賛
返信
1 返信

1,146件の閲覧回数
jpa
Contributor IV
Well, I have a solution, but I'm not sure you're going to like it. I ran into the same error under Debian 'etch'. When I moved to Fedora Core 6 the problem went away.

For what it's worth...

JPA
0 件の賞賛
返信