Error in MCF52223RM ?!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in MCF52223RM ?!

1,656件の閲覧回数
AnteOO
Contributor II

 

Hi! On page 25-25 in the MCF52223RM, it says
"

 

The ADC consists of a cyclic, algorithmic architecture using two recursive sub-ranging sections (RSD#1

and RSD#2), shown in

clock, resulting in an overall conversion rate of two bits per clock cycle. Each sub-ranging section is

designed to run at a maximum clock speed of 5.0 MHz. Thus a complete 12-bit conversion takes 6 ADC

clocks (1.2ms), not including sample or post processing time."

 

 

I'm guessing that it should be µs, instead of ms :smileywink:

 

just in case you want to change it!

I found no other way of contacting freescale, save starting a support errand...

ラベル(1)
0 件の賞賛
返信
1 返信

1,369件の閲覧回数
scifi
Senior Contributor I

Hi!

 

You are not the first one to notice this:

 

https://community.freescale.com/message/62324#62324

 

Thanks for sharing, anyway.

0 件の賞賛
返信