Encapsulate code into  header and trailer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Encapsulate code into  header and trailer

3,179件の閲覧回数
SVC1
Contributor I

Hi,

 I am trying to encapsulate the code into a header and trailer. Therefore, I used the following technique:

In vectors.s, I have

Code:
 _DEF_SW_VERSION .set 5407 .global VECTOR_TABLE .global _VECTOR_TABLE .global start .extern _asm_startmeup .extern ___SP_INIT .extern _asm_exception_handler .extern _asm_isr_handler .extern _dbug_sc_handler .def _header .def _header_end .def _trailer .def _trailer_end .text "header"/* * Exception Vector Table */VECTOR_TABLE:_VECTOR_TABLE:INITSP:  .long ___SP_INIT  /* Initial SP   */INITPC:  .long 0x400   /* Initial PC   */vector02: .long _asm_exception_handler /* Access Error  */vector03: .long _asm_exception_handler /* Address Error  */vector04: .long _asm_exception_handler /* Illegal Instruction */vector05: .long _asm_exception_handler /* Divide by Zero  */vector06: .long _asm_exception_handler /* Reserved   */vector07: .long _asm_exception_handler /* Reserved   *//* … etc … */vectorFF: .long _asm_isr_handlerstart: .long 12351236h       ; 2 word header signature .long _DEF_SW_VERSION ; 2 words for version identification .word 0               ; 1 word for n_words .word 0               ; 1 word for checksum .word 0, 0, 0, 0      ; 4 words for future expansion move.w #0x2700,SR jmp  _asm_startmeup_header_end:/* -------- Trailer ------*/.text "trailer"_trailer:  .long 0ABCEABCFh        ; 2 word trailer signature      .word 0, 0, 0, 0, 0, 0  ; 6 words for future expansion _trailer_end:/* End of vector.s */ .end


 In the memory, I can see header’s signature (12351236h) followed by (after some data) the trailer’s signature.

How can I make the trailer part go at the end of the code in memory?

Thanks,

Simon

 

 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,984件の閲覧回数
admin
Specialist II

The sequence of the relocatable modules in the target memory is defined in the linker command line.

In your case, you need to place the object file of the trailer module to the end of the linker's object file list.

 

0 件の賞賛
返信

1,984件の閲覧回数
SVC1
Contributor I
How can I do that. In vector.s, I have
 
Code:
_DEF_SW_VERSION    .set 0x7777 .global VECTOR_TABLE .global _VECTOR_TABLE .global start .global _start .global _header .global _header_end  .global _trailer .global _trailer_end .extern _startup .extern ___SP_AFTER_RESET   .extern _asm_exception_handler .extern _asm_isr_handler .text /* * Exception Vector Table */    VECTOR_TABLE:_VECTOR_TABLE:INITSP:  .long ___SP_AFTER_RESET INITPC:  .long _start   vector02: .long _asm_exception_handler /*..... ........ .....*/vectorFF: .long _asm_isr_handler/* ------------------------------- */ .text "header"_header:  .long 12351236h ; signature .long _DEF_SW_VERSION ; version .long 0  ; Number of words .long 0  ; Checksum_header_end:/* ------------------------------- */_start:start: move.w #0x2700,SR jmp  _startup  /* ------------------------------- */ .text "trailer"_trailer: .long 0ABCEABCFh /* signature     */ .long 0, 0, 0,  /* for future expansion */_trailer_end:/* ------------------------------- */  .end

 
How do I insert _header and _trailer into the lcf linker file?
 
Thanks in advance,
Simon
 
0 件の賞賛
返信

1,984件の閲覧回数
admin
Specialist II
To place the trailer code to the end of the application code, move the trailer code into separate file trailer.s.
List the trailer.o at the end of linker list of the object files.
I am not familiar with any compiler directive, which provides ordering of the object files in the linker list. You can edit the linker command line manually.

The alternative (dirty) way is to place label "_trailer:" at constant (big enough) address with .org directive.


0 件の賞賛
返信