Dragonball I/O drive capabilities

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Dragonball I/O drive capabilities

1,460 次查看
Tim301
Contributor I

Hi Folks,

 

I've been having a hard time finding any information about the

electricals of the Dragonball.

 

Anybody know what the drive capabilities of individual I/O pins are?

 

Thanks,


Tim

标签 (1)
0 项奖励
回复
1 回复

1,057 次查看
chrishartwell
Contributor I

See table 6 of the reference manual.

 

According to Table 6 (Maximum and Minimum DC Characteristics) of the i.MXL Datasheet (MC9328MXL, Rev. 8, 12/2006) :

VOH - Output high voltage (IOH = 2.0 mA) = 0.7 * VDD as minimum.

This means 2mA of current load as minimum.

VOL - Output low voltage (IOL = -2.5 mA) = 0.4 V as maximum.

That is – 2.5 mA as minimum.

 

http://www.freescale.com/files/32bit/doc/data_sheet/MC9328MXL.pdf

0 项奖励
回复