Does CodeWarrior Support USB Debugging?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does CodeWarrior Support USB Debugging?

6,563 次查看
Reallin
Contributor II
I just found a document about Jtag debugging, does CW support USB?
If it does,where can i find the informention about this?
标签 (1)
6 回复数

3,492 次查看
Reallin
Contributor II
Yes
where can i find it's help document?
0 项奖励
回复

3,492 次查看
mpeters
Contributor I

I don't believe that there are any help documents for the USB/BDM interface. It was developed by P&E Microcomputer Systems (www.pemicro.com), but it's just the interface from your IDE to the BDM header on your development board.

Is there something specific you want to know about the USB/BDM interface?

-mp

0 项奖励
回复

3,492 次查看
takaoyamada
Contributor IV

Greetings,

P&E does have documentation for all of the hardware interfaces. You need to go to our support -> "documentation & downloads"  to find them.

Here is a link to all doc and downloads for the USB BDM Multilink:

P&E Microcomputer Systems - USB BDM Multilink Cable - USB BDM Interface cable for the 68HC(S)12(X) a...

Takao Yamada

P&E Microcomputer Systems

0 项奖励
回复

3,492 次查看
mnorman
NXP Employee
NXP Employee
It supports the use of the P&E USB BDM cable. Is that what you mean?
0 项奖励
回复

3,492 次查看
Reallin
Contributor II
By the way,
My CodeWarrior is for 68k
v 7.2
0 项奖励
回复

3,492 次查看
TomE
Specialist II

Reallin Zhao writes:

> My CodeWarrior is for 68k

For what CPU? Does your CPU support JTAG? If it is a real 68k (meaning MC68000) then that chip doesn't have a debug port.

If it is something like a 68306 then that chip has JTAG, but nothing in the manual documents its use for debugging.

The "USB BDM Multilink" mentioned ONLY works on the 6 pin debug connector on the  Freescale HCS08, HC(S)12(X), RS08, and ColdFire V1 microcontrollers. It doesn't work on the V2, V3 or V4 ColdFire CPUs which have a 26-pin connector. For them you need the "USB Multilink Universal", as it supports Freescale HCS08, HC(S)12(X), S12Z, RS08, ColdFire V1/+V1, ColdFire V2-4*, Qorivva 5xxx, and Kinetis ARM microcontrollers (but costs $100 more at $199).

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137

If you really mean "68k" and the only ones that can support JTAG debugging are the MC683xx series, then you need the 'USB Multilink Universal FX" which costs another $200 ($399):

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320143

There also seem to be older parallel port cables, but you have to get separate 3.3V and 5V ones, and then you have to find an old computer with a parallel port.

Tom