Crosscompiler or build a crosscompiler for MCF5329

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Crosscompiler or build a crosscompiler for MCF5329

2,901 Views
Knopf
Contributor I
Is there a gcc for MCF5329?
 
Is there a posibility for buid a crosscompiler with linux?
 
But about his i have never done but i am using linux.
 
Has someone expierience about that and can halp me?
 
best thanks for help
 
Ralf
Labels (1)
0 Kudos
Reply
1 Reply

1,026 Views
DavidS
NXP Employee
NXP Employee

Hi Ralf,

There is about to be a uClinux BSP release for the MCF5329/73 families that has the gcc tool set included.

Keep checking on http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127268688033202A9 for the release.

If just looking for gnu tools goto http://www.codesourcery.com/gnu_toolchains/coldfire/ .

They have the most recent tool chain that then gets integrated into our ColdFire BSP's.

Regards, David

0 Kudos
Reply