Could not set PC to entry point debug error for P&E USB ColdFire Multilink tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could not set PC to entry point debug error for P&E USB ColdFire Multilink tool

2,298 Views
Johnny_zhou
Contributor I

I could not enter into debug mode and there is 'Could not set PC to entry point' pop-up.  I also try to debug via NXP website demo AN2892SW. That is same error. It is a old project and debug succesfully before. Debug tool  and hardware board is good. I don't know what this error mean.  Would you give me some direction to remove it? Thanks.

Debug tool - P&E USB ColdFire Multilink tool

MCU - MCF5234

IDE - Codewarrior V5.7

PC environment -  Vmware windows XP

Johnny_zhou_0-1700556781831.png

 

 

Tags (1)
0 Kudos
Reply
2 Replies

2,286 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

Is there a way to test this situation without vmware, It seems the computer is confusing about the entry point and where is located.

Regards

0 Kudos
Reply

2,261 Views
Johnny_zhou
Contributor I

I change try without Vmware. There is no error indication and could enter into debug view. But I could not step into or step over normally. I download demo AN2892SW

In addition, after download demo, there are  function redeclaration build error. I undefine redeclaration function and build successfully and debug it not normally. I don't know why?  Thanks.

0 Kudos
Reply