Connecton Problem MC5485EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connecton Problem MC5485EVB

1,872件の閲覧回数
Bibhu85
Contributor I
Hi,
I started working on this kit yesterday.
I wrote a sample program and when I clicked debug , its giving an error saying it can't connect to the board.
I have connected to the board using a serial connection. Hyper terminal works fine.
I cannot connect to the board using a parallel connection since my laptop doesn't have such a port.
So I basically use a serial to USB converter, and thats a COM 15 for me.
In CodeWarrior's console debug settings, I have made the appropriate changes but I am still not able to connect.
Is there a way I could FTP or TFTP to the board. Its bare. Doesn't still have an OS or anything.
 
Thanks,
 
Bibhu
ラベル(1)
0 件の賞賛
返信
1 返信

1,171件の閲覧回数
Bibhu85
Contributor I
I tried following the quick start guide that I got with the CodeWarrior CD.
So I used CCS-SIM in the connection setting.
It gave me ccs_cf_protocol_plugin. Its licensed and a valid license key not found.
0 件の賞賛
返信