Compile with mcf5207

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compile with mcf5207

4,519 Views
jgiacomoni
Contributor II

Hi, 

I have a MCF5207, but I would like to compile c++ code with code warrior. 

How to make this ? I just would like compiler and no ide.

 

Thanks a lot.

Tags (2)
0 Kudos
Reply
5 Replies

4,345 Views
jgiacomoni
Contributor II

Hello,
or can I download the 6.4 compiler only?

 

thanks,

Jessy G;

0 Kudos
Reply

4,337 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

is better to download the 7.2v, You can download it here:

https://www.nxp.com/design/design-center/software/development-software/codewarrior-development-tools...

and you have to use the stationary project for MCF5208

regards

0 Kudos
Reply

4,461 Views
jgiacomoni
Contributor II

My compiler info is : 

My version is :
CodeWarrior C/C++ for ColdFire.
Copyright (c) 2009, Freescale Semiconductor, Inc
All rights reserved.
Version 6.0 build 2004 (build 2004)
Runtime Built: Apr 7 2010 17:53:02

0 Kudos
Reply

4,488 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If you have codewarrior 6.3 or up, you have to create the project for C++ and you can build it. And you can select the MCF5208 since it have a stationary project.

Regards

0 Kudos
Reply

4,464 Views
jgiacomoni
Contributor II
Hello ! 

Where I can download compiler ? 
0 Kudos
Reply