Coldfire V1 & V2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Coldfire V1 & V2

1,384件の閲覧回数
Eric_t
Contributor III

Hi everybody,

 

I am going to start two projects; one with Coldfire V1 (MCF51MM128CLK) and one with Coldfire V2(MCF52252AF80)

 

I have attached two schematics.

 

Could someone tell me if there is any error between the controller and debugger connector?

Also I am not sure where the ALLPST pin of coldfire V2 should be connected. 

 

Thanks

Nikos 

ラベル(1)
0 件の賞賛
返信
1 返信

1,060件の閲覧回数
TomE
Specialist II

Download every development board schematic you can find and see how things are connected. there. Copy them slavishly.

 

1.5.2 Integrated Debug Module

The device includes a new debug signal, ALLPST. This signal is the logical AND

of the processor status (PST[3:0]) signals and is useful for detecting when the

processor is in a halted state (PST[3:0] = 1111).

 

Does your debugger need DDATA[3:0] and PST[3:0]? Does it need ALLPST as well or instead?

 

Note "33.4.6 Freescale-Recommended BDM Pinout" shows 23 of the 26 pins connected. You have 13. That my be what you want, but check. Your debugger manual might clear this up.

 

I don't like your power-on circuitry. THe chip has "low voltage detect" forcing reset, but it doesn't trigger until 2.15V, and the CPU isn't rated to run at under 3.0V. I think you need an external reset generator on RSTI, so it mightn't survive or recover from a brownout.

 

Why are you adding pulldowns on all those pins? You don't need to pull any pin you can program as an output and force high or low.

 

Tom

 

0 件の賞賛
返信