Coldfire M5485EVB with just released Linux kernel, u-boot problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Coldfire M5485EVB with just released Linux kernel, u-boot problem

3,086 Views
jkimble
Contributor III

I'm using a custom board based on the M5485EVB. Biggest difference is more SDRAM (128M) and more and different Flash (64MB, Intel P33).

I've made the same type changes I made to get colilo to work (Changes CFG_CS#_BASE, MASK and CTRL in M5485EVB.h and start addresses in start.S) but I'm getting nothing. Can someone tell me if there's a common way to change these two things (flash and ram size) in u-boot. U-boots a lot more complex than colilo so I'm just not sure if I'm getting everything that needs to change with a corresponding change to the CS0_BASE address.

Thanks,

Labels (1)
0 Kudos
Reply
2 Replies

2,303 Views
fsl_linux_spt
Contributor III
U-boot is an open source project.  Freescale does not own or provide direct support for u-boot. 
 
That said, I found some info about porting u-boot to a new board:
 
 
 
 
 
 
 
-- Coray
0 Kudos
Reply

2,303 Views
jkimble
Contributor III
 
A little Google goes a long way eh? I jumped too quick to the forum. There's a lot of stuff out there for u-boot (as opposed to the vast silence I found on Colilo)....
 
Thanks,
0 Kudos
Reply