ColdFire V2 Instruction set

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ColdFire V2 Instruction set

2,312 次查看
Kremer
Contributor I
 Hi all
 
 Can any of you tell me how many instructions are available in this Coldfire V2 instruction set, including all the arithmetic for integers and FP? I would like to compare it to others RISC mcu´s available at this moment.
 
 Thank you
 
--
Alban: posts should include device in subject line

Message Edited by Alban on 2007-03-28 08:35 PM

标签 (1)
0 项奖励
回复
1 回复

1,207 次查看
JWW
Contributor V
Kremer,

General V2 information can be found at the following link:

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0162468rH3YTLC6951fgqk7SDQMY7F

This page gives you a good spot to start.

There are several V2 based Coldfire products, you will have to refer to the specific product to see which ISA (instruction set) it has.

But in general, if you want to just learn about the Coldfire arch, then
click on the "CFPRM" link.

Also here:
http://www.freescale.com/files/dsp/doc/ref_manual/CFPRM.pdf

This manual give you all the good stuff for all the ISAs for Coldfire.

Hope this helps.

-JWW
0 项奖励
回复