ColdFire TCP/IP Lite Feedback

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ColdFire TCP/IP Lite Feedback

Jump to solution
2,867 Views
TomLEE
Contributor III

Hello,

this my first developpment in Coldfire MCF52233 and I am using the M52233DEMO board with Coldfire TCP/IP Lite Stack V3.0 and V3.2.

On 3.0 version, all is working fine but with the latest version, I can not activate the UART console.

I set NPDEBUG = 1, on the demo board, the UART number is 0 so I do not modify it in CONSOLE_UART (=0).

The "printf" function don't work (ie: after reset, in main.c, printf("\n\nRunning ColdFire TCP/IP-Lite stack Revision 3.1\n"):smileywink: but I have nothing on hyperterminal.

With V3.0, it works.

 

As I have trouble to run Coldfire_Lite_UDP_client, I want to debug with UART.

 

Could you help me, please ?

Thank you,

best regards,

Thomas RETAIL.

 

PS: sorry for my english, I don't speak fluently...

Labels (1)
0 Kudos
Reply
1 Solution
1,675 Views
TomLEE
Contributor III

I have found: on InterNiche Lite Stack V3.0, the BAUDRATE = 115 200 bauds

and on V3.2, BAUDRATE was changed to 19 200 bauds !

 

View solution in original post

0 Kudos
Reply
1 Reply
1,676 Views
TomLEE
Contributor III

I have found: on InterNiche Lite Stack V3.0, the BAUDRATE = 115 200 bauds

and on V3.2, BAUDRATE was changed to 19 200 bauds !

 

0 Kudos
Reply