ColdFire Global Variables

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ColdFire Global Variables

跳至解决方案
2,937 次查看
PabloA
Contributor II

Hi, I'm starting with ColdFire Family C language and I will appreciate if somebody can help me with C structure.
I have some time programming in C for 8 bits microcontrollers using CodeWarrior V10.1 and I found my first difference between 8 bits microcontrollers and ColdFire:

When I define my variables, I use to write a header file like this:

 

#if Global_Variable//- MY_ZEROPAGE RAM from 0x0080 to 0x00FF --------------------------------------------------------------------- #pragma DATA_SEG __SHORT_SEG MY_ZEROPAGE    unsigned char SCI2_Input_Buffer [30];  unsigned char SCI2_Output_Buffer [30];  unsigned char SCI2_Input_Chr_Cnt = 0;  unsigned char SCI2_Status = 0;  unsigned char SCI2_Output_Chr_Cnt = 0;  unsigned char SCI2_Output_Chr_Limit = 0;  unsigned char *Data_Pointer;       #pragma DATA_SEG DEFAULT//- MY_RAM from 0x0100 to 0x087F --------------------------------------------------------------------- #pragma DATA_SEG MY_RAM    unsigned char Function_Request = 0;  unsigned int Delay_Cnt = 0;   #pragma DATA_SEG DEFAULT  #endif//**************************************************************************************************************#if Extern_Variable//- MY_ZEROPAGE RAM from 0x0080 to 0x00FF --------------------------------------------------------------------- #pragma DATA_SEG __SHORT_SEG MY_ZEROPAGE    extern unsigned char SCI2_Input_Buffer [30];  extern unsigned char SCI2_Output_Buffer [30];  extern unsigned char SCI2_Input_Chr_Cnt;  extern unsigned char SCI2_Status;  extern unsigned char SCI2_Output_Chr_Cnt;  extern unsigned char SCI2_Output_Chr_Limit;  extern unsigned char *Data_Pointer;      #pragma DATA_SEG DEFAULT//- MY_RAM from 0x0100 to 0x087F --------------------------------------------------------------------- #pragma DATA_SEG MY_RAM  extern unsigned char Function_Request;  extern unsigned int Delay_Cnt; #pragma DATA_SEG DEFAULT    #endif

 

In this way I can use this variables shared with all functions.

I get MY_ZEROPAGE and MY_RAM labels from the Proyect.prm file were it specified a RAM or ROM space.

 

/* This is a linker parameter file for the mc9s08gt32a */NAMES END /* CodeWarrior will pass all the needed files to the linker by command line. But here you may add your own files too. */SEGMENTS /* Here all RAM/ROM areas of the device are listed. Used in PLACEMENT below. */    Z_RAM                    =  READ_WRITE   0x0080 TO 0x00FF;    RAM                      =  READ_WRITE   0x0100 TO 0x087F;    ROM                      =  READ_ONLY    0x8000 TO 0xFFAF;    ROM1                     =  READ_ONLY    0xFFC0 TO 0xFFCB; /* INTVECTS                 =  READ_ONLY    0xFFCC TO 0xFFFF; Reserved for Interrupt Vectors */ENDPLACEMENT /* Here all predefined and user segments are placed into the SEGMENTS defined above. */    DEFAULT_RAM,                        /* non-zero page variables */                                        INTO  RAM;    _PRESTART,                          /* startup code */    STARTUP,                            /* startup data structures */    ROM_VAR,                            /* constant variables */    STRINGS,                            /* string literals */    VIRTUAL_TABLE_SEGMENT,              /* C++ virtual table segment */    DEFAULT_ROM,    COPY                                /* copy down information: how to initialize variables */                                        INTO  ROM; /* ,ROM1: To use "ROM1" as well, pass the option -OnB=b to the compiler */    _DATA_ZEROPAGE,                     /* zero page variables */    MY_ZEROPAGE                         INTO  Z_RAM;ENDSTACKSIZE 0xF0/* VECTOR 0 _Startup /* Reset vector: this is the default entry point for an application. */

 

 

Now, where is the Proyect.prm file in CodeWarrior proyect for a ColdFire device like MCF51CN128?

Please, can you explain me how I can specify Global Variables that I can use in any function?

 

Theank you for your time.

Best regards, Pablo Suárez from Buenos Aires.

标签 (1)
0 项奖励
回复
1 解答
2,044 次查看
JimDon
Senior Contributor III

It really has little to do with the MCU's any "C" compiler will do this. In "C" this will work:

 

// My header file, globals.h:extern int gRAMVariable;
extern const int gROMVariable;

 

// Define the global variable in a "C" file. globalsl.cint gRAMVariable = 10;
const int gROMVariable = 20;

 

// In another "C" file, say function.c:#include "globals.h"int function(){
    gRAMVariable = 100;
    gROMVariable = 50; // ERROR! Can write to a const!     return gRAMVariable * gROMVariable;  }

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,044 次查看
JimDon
Senior Contributor III

There is no prm file, instead it uses an lcf file.

Unless there is some special requirement I am missing, you should not have to place globals explicitly in segments, as variables not decalred as const will just be put in RAM. Also, the ram is just a linear block of memory.

 

0 项奖励
回复
2,044 次查看
PabloA
Contributor II

Jim, Thank you for your reply.
But, how I define a variable that I want to use in all functions?

 

With 8 bits microcontrollers if I define a variable in an specific function like:

 

unsigned int variable;

 

it can be used just in this function. If I define it like this:

 

static unsigned int variable;

 

the data stored will be preserved for the next time the function will called, but I can't get the data of this variable from another function.

 

I think there is another way to specify variables or ROM segments that I don't know.

 

 

0 项奖励
回复
2,045 次查看
JimDon
Senior Contributor III

It really has little to do with the MCU's any "C" compiler will do this. In "C" this will work:

 

// My header file, globals.h:extern int gRAMVariable;
extern const int gROMVariable;

 

// Define the global variable in a "C" file. globalsl.cint gRAMVariable = 10;
const int gROMVariable = 20;

 

// In another "C" file, say function.c:#include "globals.h"int function(){
    gRAMVariable = 100;
    gROMVariable = 50; // ERROR! Can write to a const!     return gRAMVariable * gROMVariable;  }

 

0 项奖励
回复
2,044 次查看
PabloA
Contributor II

Jim, thank you for your time and interest. It was very useful.

 

Best regards!

Pablo

0 项奖励
回复