Codewarrier for microcontollers 6.2 BDM connection problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrier for microcontollers 6.2 BDM connection problem

Jump to solution
4,447 Views
senthil_epigon
Contributor II

Hi all,

     I am new to this forum, i was using codewarrier 6.1 for long time and no problem with that.  Now i moved onto 6.2 version , with this version i am facing BDM connection problem.  I have DEMOJM hardware, with it BDM port  i connected my hardware(which has codefire MCF51JM128 microcontroller), this connection works fine with 6.1 version. But with same setup,same machine connection not working with 6.2 version.    Even i tried updating 6.2 version with "patch version 6.2.2" but it is not helping.  Is is anything restricted in 6.2 or it's bug with this version.  kindly help on this issue.  thanks in advance.

Labels (1)
0 Kudos
Reply
1 Solution
2,780 Views
senthil_epigon
Contributor II

Thanks....

It works fine.

Great job.

View solution in original post

0 Kudos
Reply
6 Replies
2,780 Views
Fasteddie042
Contributor I

You are correct, the BDM port has been disabled in the future versions of Codewarror.  In fact when I contacted PE Micro about this they claimed that it was never supported...  Personally I just keep a version of CW 6.1 handy.

 

 

Message Edited by Fasteddie042 on 2009-05-15 05:44 PM
0 Kudos
Reply
2,780 Views
wrljet
Contributor II

What do we have to buy in order to debug under 6.2?

 

Bill

 

0 Kudos
Reply
2,780 Views
wrljet
Contributor II

FWIW, I got this working.  I can now use the DEMOJM board BDM header to debug my own boards with the Coldfire chip, from Codewarrior 6.2.

 

I edited one config file and copied in one older DLL from 6.1.

 

Bill

 

0 Kudos
Reply
2,780 Views
senthil_epigon
Contributor II
I would be great help,if you could share the information,that you did to make work with 6.2.
0 Kudos
Reply
2,780 Views
wrljet
Contributor II

Here's what I did.  "Works for me" as us programmers like to say.

 

I have the two versions installed in:

 

    C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.1

 

and

 

    C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.2

 

Copy the old DLL:

 

    unit_cfz_v1_version_327.dll 

 

from:

 

    C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.1\prog\P&E 

 

to:

 

    C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.2\prog\P&E

 

 

Edit:

 

    C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.2\prog\P&E\ngs_devices_cf.ini

 

In this section of the INI file for the JM128, I changed the name of the DLL from ...330... to ...327...

 

[MCUID7003]
DRIVER=unit_cfz_v1_version_
327.dll
DEVICENAME=MCF51JM128
NUM_PACKAGES=0
TRIM_TYPE=0

 

That' it.   For what it's worth, the BDM on my DEMOJM board is at Flash Version 5.79.

 

0 Kudos
Reply
2,781 Views
senthil_epigon
Contributor II

Thanks....

It works fine.

Great job.

0 Kudos
Reply