Codewarrier for microcontollers 6.2 BDM connection problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrier for microcontollers 6.2 BDM connection problem

ソリューションへジャンプ
4,499件の閲覧回数
senthil_epigon
Contributor II

Hi all,

     I am new to this forum, i was using codewarrier 6.1 for long time and no problem with that.  Now i moved onto 6.2 version , with this version i am facing BDM connection problem.  I have DEMOJM hardware, with it BDM port  i connected my hardware(which has codefire MCF51JM128 microcontroller), this connection works fine with 6.1 version. But with same setup,same machine connection not working with 6.2 version.    Even i tried updating 6.2 version with "patch version 6.2.2" but it is not helping.  Is is anything restricted in 6.2 or it's bug with this version.  kindly help on this issue.  thanks in advance.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,832件の閲覧回数
senthil_epigon
Contributor II

Thanks....

It works fine.

Great job.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
2,832件の閲覧回数
Fasteddie042
Contributor I

You are correct, the BDM port has been disabled in the future versions of Codewarror.  In fact when I contacted PE Micro about this they claimed that it was never supported...  Personally I just keep a version of CW 6.1 handy.

 

 

Message Edited by Fasteddie042 on 2009-05-15 05:44 PM
0 件の賞賛
返信
2,832件の閲覧回数
wrljet
Contributor II

What do we have to buy in order to debug under 6.2?

 

Bill

 

0 件の賞賛
返信
2,832件の閲覧回数
wrljet
Contributor II

FWIW, I got this working.  I can now use the DEMOJM board BDM header to debug my own boards with the Coldfire chip, from Codewarrior 6.2.

 

I edited one config file and copied in one older DLL from 6.1.

 

Bill

 

0 件の賞賛
返信
2,832件の閲覧回数
senthil_epigon
Contributor II
I would be great help,if you could share the information,that you did to make work with 6.2.
0 件の賞賛
返信
2,832件の閲覧回数
wrljet
Contributor II

Here's what I did.  "Works for me" as us programmers like to say.

 

I have the two versions installed in:

 

    C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.1

 

and

 

    C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.2

 

Copy the old DLL:

 

    unit_cfz_v1_version_327.dll 

 

from:

 

    C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.1\prog\P&E 

 

to:

 

    C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.2\prog\P&E

 

 

Edit:

 

    C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.2\prog\P&E\ngs_devices_cf.ini

 

In this section of the INI file for the JM128, I changed the name of the DLL from ...330... to ...327...

 

[MCUID7003]
DRIVER=unit_cfz_v1_version_
327.dll
DEVICENAME=MCF51JM128
NUM_PACKAGES=0
TRIM_TYPE=0

 

That' it.   For what it's worth, the BDM on my DEMOJM board is at Flash Version 5.79.

 

0 件の賞賛
返信
2,833件の閲覧回数
senthil_epigon
Contributor II

Thanks....

It works fine.

Great job.

0 件の賞賛
返信