Clock source for USB on MCF52223

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clock source for USB on MCF52223

2,577件の閲覧回数
Hjerrild
Contributor I
Hi, I'm a bit confused about how to USB device in the MCF52223 should be clocked.
What clock frequency should the USB device have? Is it connected to the clock tree like all the other internal devices or is it getting the clock directly from oscilator block?
 
In the MCF52223 Reference Manual Rev. 2 Figure 5-1 the USB device is not shown. Is that an error? Is the FlexCAN device replaced with USB??
 
Best Regards  Hjerrild
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,517件の閲覧回数
DrSeuss
Contributor I
The USB modual can be clocked directly from the 48 MHz external crystal or from the USB_ALT_CLK pin. It is not quite acurate to replace the CAN in the figure 5-1. There is No CAN on the mcf52223, I will correct.
0 件の賞賛
返信

1,517件の閲覧回数
giga
Contributor I
Is there an updated clock tree showing the USB module?  I am looking at Rev. 2 of the reference manual.  Also, I don't see in the data sheet where it references the USB_ALT_CLK in the pin functions as any of the primary, secondary or tertiary functions, however I do see it referenced on the demo board schematic and the USB_CTRL register.  I am trying to figure out how to drive the USB from the PLL with an 8MHz input, 80MHz core clock and 48MHz USB clock.  Is that possible?
0 件の賞賛
返信