Can you please help me and run this test on a Coldfire Linux System?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can you please help me and run this test on a Coldfire Linux System?

2,335 Views
GunnarVB
Contributor I

Hello

 

It would be great if people having a Coldfire Linux system could be kindly run the below little test for me:

http://www.apollo-core.com/sortbench.c

 

Please be so kind and download the source and compile it with -O2,

execute it and please post the result.

 

Many thanks your help is very much appreciated.

 

 

Kind regards

Gunnar

Labels (1)
0 Kudos
Reply
3 Replies

2,109 Views
TomE
Specialist II

A Bubble Sort! That's not really a good test of anything. Can you tell us why you chose it - what characteristics of the CPUs are you trying to test?

Bubble sort - Wikipedia, the free encyclopedia

http://www.cs.duke.edu/~ola/papers/bubble.pdf

jargon, node: bogo-sort

"... bubble sort, which is merely the generic *bad* algorithm."

The 32 passes you have that "benchmark" running are acting as a "cache-buster". It is stepping up through increasing data array sizes and then running through sequential data. As soon as the array is bigger than the cache the code will get slower. If this is what you want to test you could be using a far simpler benchmark.

Please post your results here. That is likely to get more responses.

The chip I'm using isn'r running Linux and doesn't have the floating point used in the time calculations. I converted it to run.

MCF5329 running at 240MHz (CF3 core, 16k combined cache):

The last column is MB/Sec courtesy of Excel:

Array =  1024  524799    bytes in 37857    usec 105.76 MB/s

Array =  2048  2098175   bytes in 150352   usec 106.47 MB/s

Array =  3072  4720127   bytes in 338087   usec 106.52 MB/s

Array =  4096  8390655   bytes in 610290   usec 104.89 MB/s

Array =  5120  13109759  bytes in 1006009  usec 99.42 MB/s

Array =  6144  18877439  bytes in 1545400  usec 93.19 MB/s

Array =  7168  25693695  bytes in 2221455  usec 88.24 MB/s

Array =  8192  33558527  bytes in 3024159  usec 84.66 MB/s

Array =  9216  42471935  bytes in 3950394  usec 82.03 MB/s

Array = 10240  52433919  bytes in 4995316  usec 80.08 MB/s

Array = 11264  63444479  bytes in 6160938  usec 78.57 MB/s

Array = 12288  75503615  bytes in 7444738  usec 77.38 MB/s

Array = 13312  88611327  bytes in 8846343  usec 76.42 MB/s

Array = 14336  102767615 bytes in 10367919 usec 75.62 MB/s

Array = 15360  117972479 bytes in 11999766 usec 75.01 MB/s

Array = 16384  134225919 bytes in 13753034 usec 74.46 MB/s

Array = 17408  151527935 bytes in 15616586 usec 74.03 MB/s

Array = 18432  169878527 bytes in 17603346 usec 73.63 MB/s

Array = 19456  189277695 bytes in 19700023 usec 73.30 MB/s

(Gave up waiting for it to complete the next one).

Here's an 800MHz ARM Cortex A4 - its memory and cache management is so good that the benchmark doesn't get slower, even at the largest array size:

-------------------------------------------------------------

SORTBENCH 1.0

-------------------------------------------------------------

Array = 1024  MB/sec = 239.64

Array = 2048  MB/sec = 238.22

Array = 3072  MB/sec = 241.01

...

Array = 31744  MB/sec = 234.54

Array = 32768  MB/sec = 234.34

I think it would be better if people could email the results to you rather than adding entries to this post.

Please add some "Contact Details" to your web site to allow this.

Your web site lacks contact details. The first and second tabs on it don't work. The "Performance" page is full of grammar and spelling errors. That doesn't give a good impression of the product:

APOLLO - High Performance Processor

aspell list < apollo | sort | uniq

APPOLLO

convirmed

GZIB

immidiates

implement (should be plural)

kep

perfromance

prim (should be "prime")

rithmetic

shoew

todays (should be "today's")

Tom


2,109 Views
GunnarVB
Contributor I

Many thanks for running the test!

>A Bubble Sort! That's not really a good test of anything.

>Can you tell us why you chose it - what characteristics of the CPUs are you trying to test?

Yes, I can explain this very well.

1) The test does some real work - sorting memory.

   Whether the algorithm is the best for sorting does not matter

   as I want to test some CPU features and not do the quickest sorting.

2) In opposite to Dhrystone the performance of the sort is depending on the CPU

   and not mainly depending of the string implementation.

3) While test loop is small, it touched some important areas of the CPU.

- Per loop iteration it does the following:

1) One Load

2) One compare

3) One conditional swap of 2 ints

4) A pointer increment

5) A counter decrement and a loop

This means the test result depends on

1) Your IPC

2) performance of cache

3) performance of branch prediction (the conditional code)

4) loop performance /acceleration of it

5) It does a memory write and load to the same cache line, which means it trigger memory hazard detection and handling of it.

This means all the important part of a CPU are involved in the test.

I've picked the test because I looked for simple test to stress the branch prediction and the loop acceleration of our Core.

Also I wanted a test which can stress the instruction fusing of our core.

Small performance tests, like this one help, me to review the pipeline behaviour.

This test in particular helped me to see a possible improvement of our instruction predecode - which improved performance.

Again many thanks for testing!

Do you by chance have a Coldfire V4 also for testing?

Did you do some changes / improvements to the code for embedded Linux for the Coldfire V3?

If yes could you please publish it?

Regarding the Website, thanks for the review but the website is a draft atm and work in progress and not public yet.

The CPU and the website are going to be launched end of this year.

By then I hope to have first of all the CPU fully polished and the website also finished.

Cheers

Gunnar

0 Kudos
Reply

2,109 Views
TomE
Specialist II

> Do you by chance have a Coldfire V4 also for testing?

No, only MCF5329 and ARM Cortex that I can easily compile and run on. We also have MCF5235 in another project, but that's in the wrong direction for your tests and I don't work on them.

> Did you do some changes / improvements to the code for embedded Linux for the Coldfire V3?

We're not running Linux at all. We are running "interrupt driven polling loops" with some generic support functions. I just changed it to use our printing macros, our hardware timer and also to pat the hardware watchdog often enough to stop the CPU from resetting.

Tom


0 Kudos
Reply